AXIS#.TUNING.INERTIA.MEASURE

Description

AXIS#.TUNING.INERTIA.MEASURE starts the Inertia Measurement algorithm. The only requirement for this feature is that the amplifier is enabled; an error will be returned if the process is started while disabled.

Once started, a short excitation will be sent to the motor and behavior monitored for ~2 seconds. After that, the data will be processed and the inertia calculated. The calculated inertia will be stored in the keyword AXIS#.LOAD.INERTIA.

If the Inertia Measurement algorithm calculates an inertia that exceeds this inertia mismatch max, the inertia will be limited to the MISMATCHMAX multiplied by AXIS#.MOTOR.INERTIA.

If the Inertia Measurement algorithm is limited by AXIS#.TUNING.INERTIA.MISMATCHMAX, its state will indicate it completed successfully but was clamped.

Versions

Action Version Notes
Implemented 02-13-01-000 

-

General Information

Type

Action

Command

Units N/A
Range N/A
Default Value N/A
Data Type N/A
See Also AXIS#.LOAD.INERTIA

AXIS#.TUNING.INERTIA.MISMATCHMAX

Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.TUNING.INERTIA.MEASURE

5021h

03h

Unsigned32

-

-

Write only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5044

1

5044 (0x13b4)

AXIS1.TUNING.INERTIA.MEASURE

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.TUNING.INERTIA.MEASURE

5044

Unsigned8

Read/Write

-